EIO0000005086.01

时钟

时钟精度:±180秒/月(室温无电误差范围)

该产品的内置时钟RTC(实时时钟)有一个极小的计时错误。误差范围在+300到-300秒/月之间,具体取决于产品的使用年限和温度波动等条件。如果您在计时至关重要的系统中使用本产品,请定期调整时钟。

注: 电池的预期使用寿命为5年,但在此之前电池可能会坏掉。电池不能由用户更换。请联系当地经销商。
反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.