80459-641-01, Rev. 10

Bridges/Repeaters

If the PLC is not in the local area of the MCC, you typically need to use a bridge/repeater to connect the communication network.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?