80459-641-01, Rev. 10

Communication Networks

There are three primary ways to connect communication networks: via bridges/repeaters, programmable logic controllers (PLCs), or a direct cable connection. Follow the applicable instructions below to make the cabling connections for your Model 6 iMCC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?