80459-641-01, Rev. 10

Network Cabling

Factory supplied network cabling is installed in accordance with UL 845 procedures and practices and routed in the bottom horizontal wireway.

To make direct connections to Class 2 or Class CM systems, install Class 2 or Class CM wiring so that it is separated from power conductors either by a barrier or a minimum space of 0.25 in. (6 mm). Route power conductors in the top horizontal wireway for maximum separation.

External network cabling must comply with Class 2 or Class CM practices under the provisions of NEC Articles 725 and 800.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?