80459-641-01, Rev. 10

Networks/Communications Overview

iMCCs contain Schneider Electric devices with communication ports. Each device has a unique internal register map. These devices may be linked together to a single point.

The Schneider Electric publications listed in iMCC-related Literature may be useful in the setup, maintenance, and regular operation of your Model 6 iMCC. Upon request, your Schneider Electric field sales representative can provide them to you in print. Or, you can download these documents from the Schneider Electric Download Center: se.com/us/en/download/ .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?