Applications Requiring Turns
There are some applications that require more than one wiring turn through the TeSys T controller:
-
All NEMA Size 4 applications require three passes through separately mounted current transformers (CTs) rated 300:5.
-
Certain two-speed constant or variable torque applications require two passes through the TeSys T conductor (CT) windows through which the motor leads must pass before being connected to the load terminals on the contactor (T1, T2, and T3). These two-speed constant or variable torque applications are for NEMA Size 1 (3/4 HP, 480 V) and all NEMA Size 2. By allowing multiple passes (turns) of the load leads through these CT windows, protection can be provided for motors with a full-load current lower than the specified operating range. Two passes of the load leads through each window effectively increase (by a multiple of two) the current that the TeSys T senses.
-
All three conductor windows must have the same number of passes, looped in the same direction, for the TeSys T to operate properly.
-
Begin passes from the load side of the TeSys T through the CT window, and return via the windows provided between the baseplate and the TeSys T. The final pass terminates on the load side of the contactor.
-
MCC units requiring multiple passes are factory supplied pre-looped with #14 wire and interposing terminal blocks.