Splicing Power Bus in Type 3R Enclosures
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
This section describes how to splice the power bus of a Type 3R enclosure (manufactured after February 1998) to the power bus of another Type 3R section. Bus splicing material is not captive if the section is equipped with offset bus. Refer to Splice Offset Horizontal Bus for instructions for splicing offset power bus in Type 3R enclosures.
To splice power bus:
-
Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
Remove the horizontal wireway covers and slide the horizontal bus barriers to gain access to the captive splice connectors (see Wireway Covers Removed and Horizontal Bus Barriers Open for the steps for removing horizontal bus barriers.
NOTE: On the integral splice bar assembly, located on the left side of each phase bus, the number of splice bars used on each phase is one greater than the number of main horizontal bus bars. The rear-most splice bar includes captive nuts. -
Remove the two left bolts from each splice assembly. Then loosen, but do not remove, the two right bolts of each splice assembly (see Loosen Bolts). If the bus has optional 85,000 A bus bracing supplied (see 85,000 A Bracing Option), also loosen the center nut of each splice assembly.
NOTE: Do not remove the two right bolts or the center bolt (if applicable) from the splice assemblies. Doing so permits spacers to fall from the splice assembly. If this occurs, re-assemble the splice bars and spacers (if applicable) in the proper order before continuing. -
Slide the splice assembly to the left until the two left holes are in line with the corresponding holes in the horizontal bus in the left section (see Slide the Splice Assembly to the Left).
-
Re-install the two left bolts through the splice assembly and into the horizontal bus (see Insert the Splice Bolts). Make sure the original conical washers are reinstalled with the concave side facing the splice bus (see Place a Conical Washer Under the Bolt Head).
-
Torque the splice connection bolts at horizontal bus connections to 31–32 lb-ft. (41.87–43.22 N•m). Torque 85 kA support nuts (if applicable) to 68–72 lb-ft. (92.2–97.6 N•m) (see Torque All Bolts).
-
Repeat steps 2–6 for all phases and the neutral bus (if supplied).
Before energizing the equipment, replace all covers and barriers.
DANGER