Splicing Offset for 3000/3200 A Horizontal Bus (Left Side of Structure Only)
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
-
In all structures with an offset or 3000/3200 A horizontal bus, splice bars are provided as a kit. This kit is packaged in a carton and shipped inside the structure. The kit contains all splice bars and mounting hardware necessary for horizontal bus splicing.
-
Use the splice kit only if splicing is to be done on the left (while facing the structure). If the splice is not on the left, remove the kit before energizing and retain it for future expansion. If a structure is to be spliced to another structure on the right, follow splicing instructions provided for that structure application.
-
On the integral splice bar assembly, located on the left side of each phase bus, the number of splice bars used on each phase is one greater than the number of main horizontal bus bars. The rear-most splice bar includes captive nuts.
To splice a horizontal bus on the left side of the structure:
-
Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
Join sections together following the appropriate steps beginning at Locating the MCC and continuing through Joining Type 3R Sections. This provides proper alignment of the horizontal bus.
-
Position the rear splice bar (the bar with captive nuts (see Splice Offset Horizontal Bus) against the back face of the rear horizontal bus bar.
-
Install a plain splice bar between each lamination of horizontal bus; install the last bar against the front face of the horizontal bus (see Splice Offset Horizontal Bus).
-
Align the four mounting holes in the splice bus and the horizontal bus.
-
Re-install the two left bolts through the splice assembly and into the horizontal bus. Make sure the original conical washers are re-installed with the concave side facing the splice bus (see Place a Conical Washer Under the Bolt Head).
-
For 600–2500 A main bus splices, torque the bolts to 31-32 lb-ft. (41.87-43.22 N•m). For 3000/3200 A main bus splices, torque the bolts to 70 lb-ft. (94.92 N•m). Torque the center nut on 85 kA braced, 3R splice bar assemblies to 70 lb-ft. (94.92 N•m).
-
Repeat steps 2–6 for each of the three horizontal bus phases.
-
Before energizing the equipment, replace all covers and barriers.
DANGER