80459-641-01, Rev. 10

Connecting the iMCC Cabling System

Units within iMCCs are connected at the factory. The cable used varies with the network type. The pin outs for the various networks are shown in Pin Outs for iMCC Networks.

Ethernet Networks use a Cat 5e RJ45 cable for connected devices.

NOTICE
LOSS OF COMMUNICATIONS
  • Do not use excessive force when making iMCC cabling connections.
  • Connections are keyed so that that pins are properly aligned.
Failure to follow these instructions can result in equipment damage.

Pin Outs for iMCC Networks

Network Cable Color
Blue White Red Black Bare
Modbus (two-wire RS-485) Signal + Signal - Not used Shield
PROFIBUS A (Neg) B (Pos)
DeviceNet CAN_L CAN_H V + V -
CANopen
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?