TeSys T Retrofit Applications
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
Remove the starter from the unit to replace the overload (melting alloy/bi-metallic). See Removing the Control Unit.
Use terminal blocks (OEKTTBML) for two-speed applications requiring multiple passes to achieve the proper adjustment range.
Restrain looped load cabling between the TeSys T controller and the terminal block with wire ties (or the equivalent) when terminal kits are used.
On 600 V Size 1 applications, add a third wire tie between the circuit breaker and contactor near the contactor line lugs. Refer to instruction bulletin 30072-013-29 for additional information.
Use copper wire only on device power and control terminals. Conductors must be sized for 60°C (140°F) or 75°C (167°F) National Electrical Code® (NEC®) ratings.
Pressure wire terminals are suitable for single conductor wire sizes #24–14, solid or stranded. Two conductor wire size is #24–18. Terminal instruction labels are located adjacent to the terminal block or on the wireway door.
DANGER