Insulation Test
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
HAZARD OF OverVoltage
Failure to follow these instructions can result in equipment damage.
|
Before an MCC is energized, take resistance measurements. Use an insulation tester (megohmmeter) with a potential of 500–1000 V. Take readings between each phase and from each phase to ground, with the branch disconnects off. Make sure the main disconnect is off during all insulation tests.
Readings from a megohmmeter with all disconnects off are typically 5–20 megohms or higher. Do not energize the MCC if readings below one megohm are found. Contact your local Schneider Electric representative. Record all megohmmeter readings for future reference. Any sudden change in resistance values (even within the acceptable range) may indicate a potentially damaged insulation system. Early detection and replacement of a potentially damaged insulation system helps avoid equipment damage.
DANGER