80459-641-01, Rev. 10

TeSys Tera Motor Management Controller

The following describes MCC starter units equipped with the TeSys Tera Motor Management Controller. Read and understand the Safety Precautions before you install, adjust, or perform maintenance on these units. For full details about MCC installation, refer to Installing the MCC.

TeSys Tera Controllers

 

Modbus

ProfiNet™

PROFIBUS

Ethernet

IEC61850  
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?