Removing the Compac™ 6 Control Unit
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
-
Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm power is off.
-
Move the operator handle to the OFF position (see Operator Handle in the OFF Position).
-
Loosen the captive fasteners (see Loosening Captive Fasteners) on the door and open it.
NOTE: Arc-rated units have additional fasteners at the top-middle and bottom-middle of the door that must be loosened to open the door (see Arc-Rated MCC Door Latches). -
Check for live circuits using a properly rated voltage sensing device. De-energize any voltage sources.
NOTE: Removal of the control station plate may be necessary to perform steps 5 and 6. To remove the control station plate:-
Loosen the captive mounting screws holding the plate to the front of the unit.
-
Remove the plate from the unit (see Control Station Plate Removed).
-
Re-attach the plate after disconnecting the load wires and control terminal block.
NOTE: Do not disconnect the wires to the control station plate.
-
-
Disconnect the power wiring from the starter terminals. Tag the terminations for re-installation.
-
Remove the top portion of the pull-apart control terminal block to which field wiring is connected.
-
Push the power leads and the top portion of the control pull-apart terminal blocks through the wiring port and into the vertical wireway.
-
Grasp the operator handle flange and press down on the structure interlock release (see Operator Handle and Interlock Release).
-
Firmly pull the unit forward to disengage the power stabs from the vertical bus. The unit should now slide freely from the MCC structure.
-
The operator mechanism-to-structure interlock helps prevent the control unit from being inserted or withdrawn with the handle in the ON position.
-
If the withdrawn unit is left in the structure, use appropriate lock-out/tag-out procedures to avoid re-loading by non-authorized personnel.
-
Remove the control unit from the structure and place it on a flat surface for servicing.
NOTE: Partial disassembly of the unit may be necessary to gain access to various electrical connections for servicing.
DANGER