80459-641-01, Rev. 10

Reassembly

To reassemble the MCC after testing and maintenance:

  1. Reinstall Compac 6 units by reversing removal steps 1–12 in Removing the Compac 6 Control Unit. Reinstall all other units by reversing removal steps 1–12 in Removing the Control Unit.

  2. Confirm the cam mechanism is in the open position; position the mounting slides of the control unit onto the slots of the mid-shelf. Slide the unit inward to engage the cam mechanism.

    For Compac 6 units, position the mounting slides of the control unit onto the slots of the mid-shelf. Slide the unit inward until the unit is halfway in, then move it inward with a quick push. This movement easily overcomes the compression of the stabs as they engage the vertical bus.

  3. Replace all barriers and cover plates and close and fasten all doors.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?