80459-641-01, Rev. 10

Maintaining the Control Unit

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.
NOTE: If a three-inch VeriSafe Absence of Voltage Tester (AVT) unit is being used to confirm that power is off, refer to the one-line diagram for the MCC to determine which parts of the MCC bus system the AVT monitors. The line side of the circuit breaker main supplying power to MCC lineup or other portions of the MCC bus system might still be powered.

Perform maintenance on control units at least annually, or more frequently if indicated by service conditions and your established maintenance policy. During installation, locate and tighten any connections that have become loose during shipment and handling, using the following procedures. If the control unit (see Control Unit) is being removed from the MCC for maintenance, start with Removing the Control Unit. If maintenance is performed with the control unit installed, start with Circuit Breaker or Disconnect Switch.

Control Unit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?