Ground Bus Splicing for Type 1, Type 12, and Type 3R
![]() |
---|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
To splice the ground bus:
-
Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
Remove ground bar bolts from the right and left sections (see Ground Splice Bar as Shipped).
-
Slide the ground splice bar into the right section, aligning the mounting holes (see Ground Bar Bolt Replaced).
-
Replace the ground bar bolts (see Ground Bar Bolt Replaced) in the right and left sections. Torque both bolts to 60–75 lb-in. (6.75–8.44 N•m).
-
Replace all covers and barriers and close all doors.