80459-641-01, Rev. 10

Splice Gaskets for Type 1 Gasketed, Type 1 Sprinkler-resistant, and Type 12 Enclosures

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying the equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • When moving MCC sections, follow the instructions in Handling the MCC. The MCC has a high center of gravity, which may cause it to tilt.
Failure to follow these instructions will result in death or serious injury.

Model 6 MCC, Type 12 sections manufactured between 1992 and 2005 included "P" shaped gaskets. When splicing to an existing MCC, refer to P Gasketing. If a P gasket is:

P Gasketing

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?