Removing the Control Unit
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
The Model 6 MCC is designed for convenient and quick control unit removal and replacement. To remove control units:
-
Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
NOTE: If a three-inch VeriSafe Absence of Voltage Tester (AVT) unit is being used to confirm that power is off, refer to the one-line diagram for the MCC to determine which parts of the MCC bus system the AVT monitors. The line side of the circuit breaker main supplying power to MCC lineup or other portions of the MCC bus system might still be powered. -
Move the operator mechanism to the OFF position (see Operator Mechanism in the OFF Position).
-
Loosen the captive fasteners (see Loosening Captive Fasteners) on the door and open it. Use a properly rated voltmeter to check for live circuits. De-energize any voltage sources.
NOTE: Arc-rated units have additional fasteners at the top-middle and bottom-middle of the door that must be loosened to open the door (see Arc-Rated MCC Door Latches). -
Release the lock-in device located at the bottom front of the unit (when supplied) by turning the screw on the front of the device until the locking pawl is parallel to the bottom of the unit (see Releasing the Lock-in Device (when supplied)).
Disconnect the power wiring from the starter terminals or, if provided, the power terminal blocks. Tag the terminations for re-installation (see Disconnected Terminal Blocks).
Remove the top portion of the pull-apart control terminal blocks to which field wiring is connected.
-
Push the power leads and the top portion of the control pull-apart terminal blocks through the wiring port and into the vertical wireway (see Power Leads and Top of Terminal Blocks Fed Through Wiring Port).
-
Pull forward on the twin handle cam mechanism located at the top front of the unit to rack the unit partially out of the structure (see Pulling the Twin Handle Cam Mechanism Forward). This action disconnects the power stabs from the vertical bus. Continue pulling forward until the handles are fully extended.
-
The operator mechanism-to-structure interlock helps prevent the control unit from being withdrawn or inserted with the handle in the ON position (see Operating the Mechanism-to-Structure Interlock).
-
If the withdrawn unit is left in the structure, use appropriate lock-out procedures to avoid re-loading by non-authorized personnel (see Locked Out Device).
-
Remove the control unit from the structure for servicing (see Control Unit Removed). In units with a full bottom plate, additional accessibility to the components and wiring can be achieved by folding the bottom plate down. To do so, lean the unit on its back, remove the two front screws, and fold the bottom plate down (see Control Unit with Bottom Plate Folded Down).
NOTE: Some MCC units can weigh up to 200 pounds (90.1 kg) and require two or more persons or special handling equipment. Lift only by supporting the bottom and/or the side panels of the unit. Refer to Proper/Improper Lifting Points for Plug-in Units Taller Than 24 in. (610 mm). -
If necessary, the door can be taken off its hinges without removing the unit. To do so, drive the hinge pins out of the hinge collars, using a small flat-bladed screwdriver or small punch (see Driving Out Hinge Pin). Remove the bottom hinge pin first.
-
When reinstalling a hinge pin, make certain that the hooked end is fully engaged into the hinge collar.
DANGER