Incoming Cable Lacing Instructions—ArcBlok 1200 Line-side Isolation Cable Vault
All cables must be laced and secured prior to installing the cable vault front cover.
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
-
For lacing material, select a sisal or hemp rope with a minimum of 2500 pounds of pull strength (625 pounds working load). Apply tape to any frayed end of the rope before lacing cables.
-
Lace the cables from all phases together in one bundle with a continuous length of rope. The ArcBlok lug cover must be in place and bolted down prior to lacing (ArcBlok Lug Cover in Place Prior to Lacing). Make sure interphase barriers are inserted in the grooves of the ArcBlok lug cover.
Lacing requires two sets of looping groups: an entry loop set and a second looping group nearer to the ArcBlok.
-
Attach one end of the rope to the cable bundle.
-
After attaching the rope to the cables, make a loop in the rope and pull the loop around the cable bundle from behind. Pull the loose end of the rope through the loop (see First Cable Lacing Loop).
-
Continue to pull the rope through the loop until the rope is tight. Continue to make a loop group of no more than two loops, wrapping the cable bundle four times.
-
Create the second loop group by pulling the rope around the cable bundle. Make a loop by pulling the loose end under the rope. Continue to pull the rope through the loop until it is tight around the cable bundle. Repeat the procedure until the cable bundle has no more than two loops, wrapping the cable bundle four times. The spacing between the upper and lower loop groups should be no less than four in. (102 mm) (see Upper and Lower Cable Lacing Groups).
-
Make sure the cable bundles do not disengage the interphase barriers from the grooves of the ArcBlok lug cover (see ArcBlok Interphase Barriers and ArcBlok Interphase Barriers and Lug Cover Grooves).
-
After the entire cable bundle has been laced, tie the ends of the ropes securely to the looping groups, then cut and tape the ends to help prevent fraying. Make sure the rope ends are not obstructing the cable vault front cover, overlapping seals, or rear panel damper.
After the entire cable bundle has been laced, tie the ends of the ropes securely to the looping groups, then cut and tape the ends to help prevent fraying. Make sure the rope ends are not obstructing the cable vault front cover, overlapping seals, or rear panel damper. -
While keeping the ArcBlok lug cover in place, remove all cover hardware.
NOTE: Make sure the interphase barriers remain inserted into the grooves of the ArcBlok lug cover (see ArcBlok Interphase Barriers and Lug Cover Grooves). -
Place the cable vault front cover on top of the ArcBlok lug cover.
-
Install 3/8–16 Keps nuts and torque them to 20–23 lb-ft. (27–31 N•m).
DANGER_0000696812.png)
_0000696831.png)