80459-641-01, Rev. 10

Inspecting the Enclosure

Perform inspection, cleaning, and any required repair activities as part of the initial maintenance of the MCC and at periodic inspection and maintenance intervals.

  1. Inspect the interior and exterior of the MCC for moisture, oil, or other foreign material. Eliminate all foreign material and clean the MCC.

  2. Clean the interior and exterior of the MCC with a vacuum cleaner. (Do not use compressed air; it redistributes contaminants to other surfaces.) Check the enclosure for damage that might reduce electrical clearances.

  3. Examine the finish of the enclosure. Touch up the paint if necessary. Replace any badly corroded or damaged enclosure parts.

  4. Check the MCC interior carefully for moisture, condensation build-up, or signs of previous wetness. Moisture can compromise electrical insulation systems and cause rapid oxidation of current-carrying parts. Inspect all conduit entrances and cracks between the enclosure panels for dripping leaks. Condensation in conduits can be a source of moisture and must not be allowed to drip onto live parts or insulating material. Take the necessary steps to eliminate moisture and seal off leaks.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?