80459-641-01, Rev. 10

Terminating Resistors

For the communication network to operate properly, terminating resistors are required on each end of the network. If your iMCC is shipped with a bridge, repeater, and/or PLC, external terminal blocks (MCT485) are included with shipment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?