80459-641-01, Rev. 10

Cables Between Shipping Splits

Connect the trunk line cables between shipping splits by aligning the keyways and plugging the pin end of the trunk cable to the socket end of the next trunk cable. Screw the coupling ring until it is hand-tight. Repeat this process until all shipping splits are connected.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?