Vent Hood Installation
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
This section contains instructions for installing a vent hood over the top plate vents on an MCC.
-
Do not install the vent hood until the MCC is in its final location.
-
Retain all hardware.
-
Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
Remove the 3/8 in. (9.525 mm) bolts, washers, and the lifting angle (see Remove the Hardware).
-
Remove the two 10-32 screws that secure the vent hood and closing plate to the top of the cabinet (see Reposition and Attach the Vent Hood).
-
Once the vent hood is removed, secure the top closing plate by reinstalling the 10-32 screws removed in step 3 (see Reposition and Attach the Vent Hood).
-
Position the vent hood on the top of the cabinet as shown.
-
Secure the vent hood in place using the two 3/8 in. (9.525 mm) bolts and washers removed in step 2. Torque the bolts to 28–33 lb-in. (3.164–3.729 N•m).
DANGER