Locating the MCC
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
MCCs are designed for use in non-hazardous locations. Choose a location for installation that is well ventilated and free from excess humidity, dust, and dirt. The temperature of the area must be no less than 0°C (32°F) and no greater than 40°C (104°F). Protect the MCC from the entrance of water or any moisture. If necessary, protect the MCC from condensation by ordering internal space heaters.
Space Requirements
Install MCCs in an area with a minimum of 3 ft. (0.9 m) of free space in front of front-of-board construction. An additional 3 ft. (0.9 m) is necessary in the rear of back-to-back construction. This free space provides adequate room to remove and install units. (More space may be required for some applications; refer to applicable local and national installation codes.) Provide at least 0.5 in. (13 mm) of space between the back of front-of-board MCCs and a wall. For damp locations, provide at least 6 in. (152 mm).
When selecting a location for the installation of an MCC, carefully consider accessibility, overhead clearances, and future expansions. Considering these factors minimizes many difficulties during this and future MCC installations.
DANGER |
|---|
|
Burn hazard from HOT GASES
Failure to follow these instructions will result in death or serious injury.
|
The shaded area (see Required Obstruction-Free Area) above the arc-rated MCC must be free from obstructions.
Aligning the MCC
Provide a smooth, level surface for installation. An uneven foundation may cause misalignment of shipping blocks, units, and doors. The surface under an MCC must be of a non-combustible material unless bottom plates are installed in each vertical section.
DANGER