Splicing Power Bus for Type 1 and Type 12 Enclosures
![]() |
---|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
To splice the power bus:
-
Turn off all power supplying this equipment before working on or inside the equipment and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
Remove the horizontal wireway covers and slide the horizontal bus barriers to gain access to the captive splice connectors (see Horizontal Wireway Covers and Bus Barriers Removed). See Appendix A—Removal and Installation of Horizontal Bus Barrier Panels for the steps for removing horizontal bus barriers.
Power Bus Splicing MCCs with Single Bar/Phase Splice Kit (600 A and 800 A, Copper Horizontal Bus, 65,000 A Short Circuit or Less, Shipped after August 2012)
-
Remove all four bolts from the integral splice bar (see Remove Bolts from Single-splice Bar).
-
Move the single splice bar to the left and align the two left holes in the splice bar with the corresponding holes in the horizontal bus on the left section (see Move and Align the Splice Bar to the Bus Holes).
-
Reinstall the four bolts into the horizontal bus on the left and right sections (see Insert Splice Bolts in the Left and Right Sections). Make sure the original conical washers are reinstalled with the concave side facing the horizontal bus (see Place a Conical Washer Under the Bolt Head).
-
Torque all bolts on both ends to 31–32 lb-ft. (41.87–43.22 N•m). (See Torquing the Bolts).
-
Return to step 2 in Splicing Power Bus for Type 1 and Type 12 Enclosures for all phases and for the neutral bus (if supplied). When all splices are complete, go to step 6.
-
Before energizing the equipment, slide the horizontal bus barriers into the closed position and replace all covers.
Power Bus Splicing MCCs with Multiple Bar/Phase Splice Kit
-
Remove the two left bolts. Loosen, but do not remove, the two right bolts on the splice assembly (see Remove the Left Bolts and Loosen the Right Bolts on the Splice Assembly).
NOTE: Do not remove the two right bolts from the splice assemblies. Doing so permits spacers to fall from the splice assembly. If this occurs, re-assemble the splice bars and spacers (if applicable) in the proper order before continuing. -
Slide the splice assembly to the left until the two left holes are in line with the corresponding holes in the horizontal bus on the left section (see Align the Splice and Bus Holes).
-
Reinstall the two left bolts through the splice bars and into the horizontal bus (see Insert the Splice Bolts); make sure the original conical washers are reinstalled with the concave side facing the splice bus (see Place a Conical Washer Under the Bolt Head).
-
Torque all bolts on both ends to 31–32 lb-ft. (41.87–43.22 N•m) (see Torque the Bolts).
-
Return to step 2 in for all phases and for the neutral bus (if supplied). When all splices are complete, go to step 6.
-
Before energizing the equipment, slide the horizontal bus barriers into the closed position and replace all covers.