80459-641-01, Rev. 10

Load and Control Wiring

The top and bottom horizontal wireways and the vertical wireway are convenient areas to run incoming line, load, and control wires (see Wiring in the Top Horizontal Wireway). Openings between sections permit wire to pass from one section into the next for interwiring.

Wiring in the Top Horizontal Wireway

Control and power wires are routed to each unit via the vertical wireway. When supplied, grommeted wire ports must be opened to route wire to the unit. The H-shaped cut pattern is pre-scored for easy opening. Using a small knife, cut through the center tabs and complete the H-shaped slice (see Vertical Wireway Grommet). When cutting, be sure not to damage the wires located near the grommet.

Vertical Wireway Grommet

Pull-apart control terminals (see Pull-apart Type Terminal Blocks) are mounted on a 35 mm DIN rail located adjacent to the wiring ports toward the front of the unit. Terminate field control wiring on the removable portion of the block.

Pull-apart Type Terminal Blocks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?