TeSys T Local Programming
DANGER |
|---|
|
Hazard of electric shock, explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
Use Local Programming for set point programming and detected error readout purposes. Configure the TeSys T by using SoMove™ software, or an HMI (display) to set the parameters.
The Parameter Settings Sheet (included with MCC order drawings) lists all the parameters that are by the factory specific to each device application. Any settings not shown on the Parameter Settings Sheet are retained at device default values. To return the TesSys T controller to its default settings, press and hold the Test / Reset button down for 16–20 seconds.
Configuring with HMI
The HMI may be supplied either as a unit-mounted option, or as a separate, handheld programming kit containing one HMI and one 3.3 ft. (1 m) connection cable.
-
Connect the HMI to the TeSys T unit:
-
If supplied as a unit-mounted option, the connection is made at the factory.
or
- Connect the programming kit via the standard, unit-mounted RJ-45 port.
-
-
Input Full Load Current (FLC):
-
Using the HMI, go to Menu>Protection Settings>Thermal>Thermal Overload>FLC1
NOTE: For additional details, refer to the TeSys T LTMCUF Control Operator Unit User Manual and the TeSys T LTMR Motor Management Controller User Guide specific to your network communication protocol. (See iMCC-related Literature for the document numbers.)
-
Configuring with SoMove Software
For details about the SoMove software, refer to the TeSys T LTMR Motor Management Control User Manual specific to your network communication protocol (See iMCC-related Literature for the document numbers.).
DANGER