Joining Type 1 Sprinkler-resistant Sections
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
This section contains instruction for joining MCC sections provided with a sprinkler-resistant enclosure.
-
Join sections together as described in Joining Type 1, Type 1 Gasketed, and Type 12 Sections.
See Removing the Lifting Angles and Hardware for steps 2 and 3.
-
Uninstall and discard the lifting angles (A) by removing the 3/8-in bolts and washers (B) securing them.
-
Remove the 10-32 screws (C) on top of the MCC section closest to the sides of the MCC sections on which the drip hood splice plate will be installed.
See Installing the Drip Hood Splice Plate for steps 4 and 5.
-
Install the drip hood splice plate (D) by reusing the hardware removed in steps 2 and 3.
-
Install the rest of the hardware removed in step 2.
DANGER