Assign Autoupdaters

Continuing from the previous topic and having assigned the field model name, it is time to assign the autoupdater.
  1. In ArcCatalog, expand your geodatabase until you find the feature class you want to configure.
  2. Right-click the feature class and choose ArcFM Properties Manager.
  3. Click the Field Info tab.
  4. Click the field to highlight it in blue. Then under Field Properties, locate the autoupdater in the drop-down.

  5. Click OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?