Select License

The Licenses tab allows you to choose an Esri license.

TIP: It is recommended that the user has local access to the license for Geodatabase Manager. This ensures that Geodatabase Manager has access to a license even if the network is down.
  1. Ensure you have the correct service selected in the Available Services window.
  2. Select the Licenses tab.

    Toggle image of Licenses tab

  3. Select a radio button to choose an Esri license: ArcGIS for Desktop Advanced, ArcGIS for Desktop Standard, or ArcGIS Engine with Geodatabase Editing.
  4. Click Apply to save changes and retain the Geodatabase Manager window. Click OK to save changes and dismiss the window. Click Close to dismiss the window. You will be prompted to save changes before closing.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?