Conductor (primary and secondary)
Event |
Autoupdater |
|
---|---|---|
On Feature Create |
ArcFM Create Feeder Object |
|
On Feature Update |
ArcFM Update Feeder Object or ArcFM Update UG Feeder Object |
|
On Feature Delete |
ArcFM OH (or UG) - Delete Feeder Conductor/Units |
|
Before Feature Split |
ArcFM Save Related Objects (Optional. This AU is available only if a relationship exists) |
|
On Feature Split |
ArcFM Split Feeder Object |
|
After Feature Split |
ArcFM Restore Related Objects (Optional. This AU is available only if a relationship exists) |
|
Assign the following autoupdater to secondary conductor classes if you want secondary conductors downstream of a transformer to inherit the transformer's LowSideVoltage value. If the LowSideVoltage value doesn't exist (and the functionality is configured) or the AU is assigned to the primary conductor, then the downstream secondary conductors inherit the OperatingVoltage value from the transformer. This autoupdater fires on the On Feature Update event only when the shape of the line is modified. |
||
On Feature Create |
ArcFM Inherit Operating Voltage |
|
Optional: The following autoupdaters are required only if you have a multi-tiered network. |
||
On Feature Create |
Remove the ArcFM Create Feeder Object AU and assign these:
|
|
On Feature Update |
Remove the ArcFM Update Feeder Object AU and assign these:
|