Primary Meter

Object Model names: TRANSFORMER

Field Model names:

Field

Field Model Name

Properties

FeederID

FEEDERID

Field Info Tab:

Reset After Create = Yes

FeederID2

FEEDERID2

Field Info Tab:

Reset After Create = Yes

FeederInfo

FEEDERINFO

Field Info Tab:

Editable = No

Reset After Create = Yes

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

Field Info Tab:

Reset After Create = Yes

PhaseDesignation

PHASEDESIGNATION

 

Optional: The following fields are required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network. The CircuitSourceID and Subsource fields should be added to all junction classes eligible to represent subsidiary sources.

ParentCircuitSourceGUID

PARENTCIRCUITSOURCEGUID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

PARENTCIRCUITSOURCEID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

CircuitSourceGlobalID

Global ID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

CircuitSourceGUID

GUID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

CircuitSourceID

CIRCUITSOURCEID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

Subsource

SUBSOURCE

 

Field Info Tab:

Visible = Yes

Editable = Yes

Reset After Create = Yes

FacilityID

FACILITYID

Field Info Tab:

Visible = Yes

Editable = Yes

Reset After Create = No

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?