Copy Design

Allows you to create a copy of an existing design.

Enabled

  • The node passed to this subtask is a design node.

  • The design has been opened in ArcMap and saved (creating an associated version).

  • The WMSUseWRVersions value in the MM_PX_CONFIG table is set to 0. If this value is set to 1 the Copy Design subtask is disabled.

Execute

  1. User interface prompts user for setup information.

  2. Creates WR (if user specified "create new WR").

  3. Creates new design(s) based on number of copies entered by user.

  4. Copies the contents of the original design to the new design(s) depending on the setup information entered.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?