Conduit Feature Class

The Conduit feature class represents the conduit in your underground system into which cables may be placed.

This feature class and its related fields can be named whatever you choose. Minerville contains the examples below. The Conduit feature class requires that you create the following fields with the listed data types:

Alias: Conduit

Type of features: ArcFM Simple Edge Feature or Complex Edge Feature

Geometric network: UndergroundNetwork

Field

Data Type

Default Value

Domain

Length/Precision

DuctBankConfiguration

Blob

N/A

DuctBankHeight

Long Integer

DuctBankWidth

Long Integer

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?