Open Express Design

Opens the selected design for editing in Designer Express.

Enabled

  • An express design node must be selected.

  • MMWorkflowManager must be the current extension.

  • Workflow Manager must be opened from Designer and visible.

Execute

  1. Gets the express design.

  2. Determines whether the express design should be opened as View Only.

  3. Creates the workspace for the express design.

  4. Opens the express design and updates the MM_PX_Versions table to indicate the design exists.

  5. Sets the PxApplication on the Process Framework Task Tool extension.

  6. Enables the Active Annotation Target tool.

  7. Disables the Stored Items tool.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?