Configure Display Name Object
Custom display name objects allow you to include multiple attributes in the display name. If you have created a custom display name object, it can be assigned to features or related objects on the Field Display tab of the ArcFM Solution Properties Manager. Select a custom display name object from the Display Name Object field. Any value selected in this field overwrites what is selected in the primary display field.
Sample Display Name Objects
Sample display name objects are available on the following feature/object classes with the ArcFM installation: CPSystem, DistributionMain, GasValve, Transformer, TransformerUnit. These samples require the following model names be assigned:
CPSystem Display Name Object
Model Name: CPSYSTEM
Field Model Names:
Field |
Field Model Name |
---|---|
ID |
ID |
ProtectionType |
PROTECTIONTYPE |
Distribution Main Display Name Object
Model Name: DISTRIBUTIONMAIN
Field Model Names:
Field |
Field Model Name |
---|---|
OperatingPressure |
OPERATINGPRESSURE |
NominalDiameter |
PIPEDIAMETER |
Material |
MATERIAL |
Valve Display Name Object (Gas and Water)
Model Name: VALVE
Field Model Names:
Field |
Field Model Name |
---|---|
FacilityID |
FACILITYID |
ValveSize |
VALVESIZE |
Material |
MATERIAL |
Transformer Display Name Object
Model Name: TRANSFORMER
Field Model Names:
Field |
Field Model Name |
---|---|
FacilityID |
FACILITYID |
PhaseDesignation |
PHASEDESIGNATION |
RatedKVA |
RATEDKVA |
Transformer Unit Display Name Object
Model Name: TRANSFORMERUNIT
Field Model Names:
Field |
Field Model Name |
---|---|
FacilityID |
FACILITYID |
PhaseDesignation |
PHASEDESIGNATION |
RatedKVA |
RATEDKVA |
Assign Display Name Objects
Once you have created a custom display name object or configured the samples provided with the ArcFM install, the display name objects must be assigned.
- Select a feature or object class in the Catalog Tree.
- Click the ArcFM Properties Manager
button on the ArcFM Solution toolbar OR right-click a feature class and select ArcFM Properties Manager.
- Select the Field Display tab.
- When a custom display name object is registered in the correct category, it will appear in the Display Name Object field. Select a value from the Display Name Object pulldown menu. The example depicts selecting Valve Display Namer from the Display Name Object pulldown. This value overwrites what is selected in the Primary Display Field.
- You must select a value for the Primary Display Field as well. This value is always used by the ArcFM Display Field locator.
- Click Apply to save edits and retain the Properties Manager OR click OK to save edits and dismiss the Properties Manager.