Assign Model Names

Use this topic to assign object class and field model names.

Busbar

Object class model name: SPLITTARGET

Field

Field Model Name

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

FacilityID

FACILITYID

PhaseDesignation

PHASEDESIGNATION

OperatingVoltage

OPERATINGVOLTAGE

FdrMgrNonTraceable

FDRMGRNONTRACEABLE

MeasuredLength

MEASUREDLENGTH

IMPORTANT: The MEASUREDLENGTH field model name is optional. If assigned, it informs the total length calculation performed by the Find Feeder Statistics tab in regard to the length of the feeder. If the model name is not assigned, the Find Feeder Statistics tab defers to the GIS length instead.

CircuitSource

Object class model name: CIRCUITSOURCE

Field

Field Model Name

FeederID

FEEDERID

FeederName

FEEDERNAME

SubstationID

SUBSTATIONID

FeederSourceInfo

FEEDERSOURCEINFO

CircuitSourceID

Object class model name: CIRCUITSOURCEID

Field

Field Model Name

FeederLevel

FEEDERLEVEL

FeederName

FEEDERNAME

ObjectID

CIRCUITSOURCEID

DynamicProtectiveDevice, Switch

DynamicProtectiveDevice object class model names: FDRMGRPROTECTIVE, PROTECTIVE

Switch object class model name: SWITCH

Field

Field Model Name

CircuitSourceID

CIRCUITSOURCEID

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

FacilityID

FACILITYID

GangOperated

FDRMGRGANGOPERATED

NormalPosition_A

NORMALPOSITION_A

NormalPosition_B

NORMALPOSITION_B

NormalPosition_C

NORMALPOSITION_C

PhaseDesignation

PHASEDESIGNATION

Subsource

SUBSOURCE

Fuse, OpenPoint

Fuse object class model names: FDRMGRPROTECTIVE, PROTECTIVE

OpenPoint object class model name: SWITCH

Field

Field Model Name

CircuitSourceID

CIRCUITSOURCEID

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

FacilityID

FACILITYID

NormalPosition_A

NORMALPOSITION_A

NormalPosition_B

NORMALPOSITION_B

NormalPosition_C

NORMALPOSITION_C

PhaseDesignation

PHASEDESIGNATION

Subsource

SUBSOURCE

PrimaryMeter

Object class model name: TRANSFORMER

Field

Field Model Name

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

FacilityID

FACILITYID

PhaseDesignation

PHASEDESIGNATION

Subsource

SUBSOURCE

CircuitSourceID

CIRCUITSOURCEID

PriOHElectricLineSegment, PriUGElectricLineSegment, SecOHElectricLineSegment, SecUGElectricLineSegment

Object class model name: SPLITTARGET

Field

Field Model Name

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

FacilityID

FACILITYID

PhaseDesignation

PHASEDESIGNATION

OperatingVoltage

OPERATINGVOLTAGE

MeasuredLength

MEASUREDLENGTH

IMPORTANT: The MEASUREDLENGTH field model name is optional. If assigned, it informs the total length calculation performed by the Find Feeder Statistics tab in regard to the length of the feeder. If the model name is not assigned, the Find Feeder Statistics tab defers to the GIS length instead.

ServicePoint

Object class model names: FDRMGRLOADPOINT, SERVICEPOINT

IMPORTANT: The SERVICEPOINT class model name informs the service count in the Find Feeder Statistics tab.

Field

Field Model Name

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

FacilityID

FACILITYID

PhaseDesignation

PHASEDESIGNATION

Transformer

Object class model name: TRANSFORMER

Field

Field Model Name

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

FacilityID

FACILITYID

PhaseDesignation

PHASEDESIGNATION

LowSideVoltage

LOWSIDEVOLTAGE

RatedkVA

RATEDKVA

IMPORTANT: The Find Feeder Statistics tab looks to fields assigned PHASEDESIGNATION and RATEDKVA for its calculations. It first looks to these fields on the Transformer Unit. If they do not exist or are not populated there, it looks to the fields with these field model names on the Transformer instead.

TransformerUnit

Object class model name: TRANSFORMERUNIT

Field

Field Model Name

RatedKVA

RATEDKVA

PhaseDesignation

PHASEDESIGNATION

IMPORTANT: The Find Feeder Statistics tab looks to fields assigned PHASEDESIGNATION and RATEDKVA for its calculations. It first looks to these fields on the Transformer Unit. If they do not exist or are not populated there, it looks to the fields with these field model names on the Transformer instead.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?