Add Model Names
Add model names to domains by right-clicking the geodatabase and selecting Properties. Note that some of the model names listed below may exist in other domains (e.g., SYMBOLROTATION, INSETFRAMESOURCE may exist in Domain Independent Field Model Names domain). You may assign these model names from a different domain or add them to the electric domains mentioned below. The various domains are primarily to help you organize your model names logically.
Class Model Names
Add the following model names to the Electric Object Class Model Name domain. Some may already exist. They must have the exact spelling as shown.
MANHOLEFEATURESNAP
STRUCTURE
UFMANCHOR
UFMANNOTATION
UFMDIMENSION
UFMDUCT
UFMDUCTBANK
Field Model Names
Add the following field model names to the Electric Field Model Name domain. Some may already exist. They must have the exact spelling as shown.
DUCTAVAILABILITY
DUCTID
DUCTMATERIAL
DUCTNAME
DUCTOCCUPIED
DUCTSIZE
FACILITYDIAGRAM
FACILITYID
HASSUBDUCTS
PHASEDESIGNATION
SYMBOLROTATION (should be in the Domain Independent Field Model Name domain)
INSETFRAMETITLE (should be in the Domain Independent Field Model Name domain)