Misc Network Features
Object Model Name: none
Field Model Names:
Field |
Field Model Name |
Properties |
---|---|---|
FeederID |
FEEDERID |
Field Info Tab: Reset After Create = Yes |
FeederID2 |
FEEDERID2 |
Field Info Tab: Reset After Create = Yes |
FeederInfo |
FEEDERINFO |
Field Info Tab: Editable = No Reset After Create = Yes |
ElectricTraceWeight |
MMELECTRICTRACEWEIGHT |
Field Info Tab: Reset After Create = Yes |
PhaseDesignation |
PHASEDESIGNATION |
|
Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network. |
||
ParentCircuitSourceGUID |
PARENTCIRCUITSOURCEGUID |
Field Info Tab: Reset After Create = Yes |
Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager. |
||
ParentCircuitSourceID |
PARENTCIRCUITSOURCEID |
Field Info Tab: Visible = Yes Editable = No Reset After Create = Yes |
FacilityID |
FACILITYID |
Field Info Tab: Visible = Yes Editable = Yes Reset After Create = No |