EDM Property Type

Use the EDM Property Type to indicate that a field in an EDD table carries site conditions data. This field property is available on the Field Info tab of the ArcFM Properties Manager for all fields in a table that carries the EXTENDEDDATADEFINITION model name.

NOTE: While the Description field has an EDM Property Type of General, no other EDM fields may have this property type. The General property type is not supported by Designer. Assign all custom EDM fields a property type of Site Conditions.

Site Condition properties appear on the Site Conditions tab in Workflow Manager.

General properties appear elsewhere. For example, the Design Name and Description for a design are extended data. They appear on the Design tab in Workflow Manager (highlighted in red below).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?