Assign Model Names
Extended Feeder Manager is configured, like other ArcFM components, by assigning model names and autoupdaters to network features. This step requires that you assign model names and field model names to your feature classes. It is easiest to assign all of the model names and field model names for a feature class rather than assigning all of the model names then all of the field model names.
BusBar:
Field |
Field Model Name |
Field Info |
FacilityID |
FACILITYID |
Reset After Create =
No |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create =
Yes |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create =
Yes |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
CircuitSourceID Object Class:
Object Model Name: CIRCUITSOURCEID
Field |
Field Model Name |
Field Info |
GlobalID |
CIRCUITSOURCEGLOBALID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceGUID |
CIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
FeederLevel |
FEEDERLEVEL |
|
FeederName |
FEEDERNAME |
|
ObjectID |
CIRCUITSOURCEID |
|
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes |
RelatedFeatureClassName |
RELATEDFEATURECLASSNAME |
|
RelatedObjectID |
RELATEDOBJECTID |
|
SubstationID** |
SUBSTATIONID |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
**This field is required ONLY for Responder and Network Adapter/DMS implementations. It will not be maintained automatically.
Conductors (primary and secondary):
Field |
Field Model Name |
Field Info |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
Delivery Point and Generator:
Field |
Field Model Name |
Field Info |
CircuitSourceGUID° |
CIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceGlobalID° |
CIRCUITSOURCEGLOBALID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceID° |
CIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
Subsource |
SUBSOURCE |
Reset After Create = Yes Visible = Yes Editable = Yes |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
° Use CircuitSourceID if you plan to use object IDs instead of global IDs. Use CircuitSourceGlobalID and CircuitSourceGUID if you plan to use global IDs instead of object IDs. If you try to assign both object IDs (CircuitSourceGlobalID) and global IDs (CircuitSourceGlobalID and CircuitSourceGUID) to a feature, it will not work with Feeder Manager.
Misc Network Features:
Field |
Field Model Name |
Field Info |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
Network Junctions:
Field |
Field Model Name |
Field Info |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
Open Point:
Field |
Field Model Name |
Field Info |
CircuitSourceGUID° |
CIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceGlobalID° |
CIRCUITSOURCEGLOBALID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceID° |
CIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
Subsource |
SUBSOURCE |
Reset After Create = Yes Visible = Yes Editable = Yes |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
° Use CircuitSourceID if you plan to use object IDs instead of global IDs. Use CircuitSourceGlobalID and CircuitSourceGUID if you plan to use global IDs instead of object IDs. If you try to assign both object IDs (CircuitSourceGlobalID) and global IDs (CircuitSourceGlobalID and CircuitSourceGUID) to a feature, it will not work with Feeder Manager.
PF Correcting Equipment:
Field |
Field Model Name |
Field Info |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
Primary Meter:
Field |
Field Model Name |
Field Info |
CircuitSourceGUID° |
CIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceGlobalID° |
CIRCUITSOURCEGLOBALID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceID° |
CIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
Subsource |
SUBSOURCE |
Reset After Create = Yes Visible = Yes Editable = Yes |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
Protective Devices (Dynamic Protective Device and Fuse):
Field |
Field Model Name |
Field Info |
CircuitSourceGUID° |
CIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceGlobalID° |
CIRCUITSOURCEGLOBALID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceID° |
CIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
Subsource |
SUBSOURCE |
Reset After Create = Yes Visible = Yes Editable = Yes |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
° Use CircuitSourceID if you plan to use object IDs instead of global IDs. Use CircuitSourceGlobalID and CircuitSourceGUID if you plan to use global IDs instead of object IDs. If you try to assign both object IDs (CircuitSourceGlobalID) and global IDs (CircuitSourceGlobalID and CircuitSourceGUID) to a feature, it will not work with Feeder Manager.
Service Point:
Field |
Field Model Name |
Field Info |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
Streetlight:
Field |
Field Model Name |
Field Info |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
Switch:
Field |
Field Model Name |
Field Info |
CircuitSourceGUID° |
CIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceGlobalID° |
CIRCUITSOURCEGLOBALID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceID° |
CIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
Subsource |
SUBSOURCE |
Reset After Create = Yes Visible = Yes Editable = Yes |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
° Use CircuitSourceID if you plan to use object IDs instead of global IDs. Use CircuitSourceGlobalID and CircuitSourceGUID if you plan to use global IDs instead of object IDs. If you try to assign both object IDs (CircuitSourceGlobalID) and global IDs (CircuitSourceGlobalID and CircuitSourceGUID) to a feature, it will not work with Feeder Manager.
Transformer:
Field |
Field Model Name |
Field Info |
CircuitSourceGUID° |
CIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceGlobalID° |
CIRCUITSOURCEGLOBALID |
Reset After Create = Yes Visible = Yes Editable = No |
CircuitSourceID° |
CIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
Subsource |
SUBSOURCE |
Reset After Create = Yes Visible = Yes Editable = Yes |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.
° Use CircuitSourceID if you plan to use object IDs instead of global IDs. Use CircuitSourceGlobalID and CircuitSourceGUID if you plan to use global IDs instead of object IDs. If you try to assign both object IDs (CircuitSourceGlobalID) and global IDs (CircuitSourceGlobalID and CircuitSourceGUID) to a feature, it will not work with Feeder Manager.
Voltage Regulator:
Field |
Field Model Name |
Field Info |
FacilityID |
FACILITYID |
Reset After Create = No Visible = Yes Editable = Yes |
ParentCircuitSourceID* |
PARENTCIRCUITSOURCEID |
Reset After Create = Yes Visible = Yes Editable = No |
ParentCircuitSourceGUID* |
PARENTCIRCUITSOURCEGUID |
Reset After Create = Yes Visible = Yes Editable = No |
*Use ParentCircuitSourceID if you plan to use object IDs instead of global IDs. Use ParentCircuitSourceGUID if you plan to use global IDs instead of objects IDs. Do not assign both of these fields to the same feature or the feature will not work with Feeder Manager.