TransformerUnit Object Class

Optional:

The following object class is required if you wish to view the Total RatedkVA for an electric Trace. A field model name on the Transformer class is required as well.

TransformerUnit Object Class

Object Model names: TRANSFORMERUNIT

Field Model names:

Field

Field Model Name

RatedkVA

RATEDKVA

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?