Configure ArcFM Phase Swap
The Phase Swap tool allows users to switch a branch of existing energized feeder from one phase to another. The following model name and field model names must be assigned. In addition, this tool also requires configuration of Feeder Manager (see below).
Model Name
|
Feature Class |
Model Name |
|---|---|
|
TransformerUnit |
TRANSFORMERUNIT |
Field Model Names
|
Feature Class |
Field |
Field Model Name |
|---|---|---|
|
Transformer |
RatedkVA |
RATEDKVA |
|
TransformerUnit |
RatedkVA |
RATEDKVA |
This tool requires configuration of Feeder Manager, which includes the following field model names:
|
Feature Class |
Field |
Field Model Name |
Domain |
|---|---|---|---|
|
Any feature class that may participate in Phase Swap |
Phase Designation |
PHASEDESIGNATION |
On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase. |
|
Any switchable device that may participate in Phase Swap |
NormalPosition_A |
NORMALPOSITION_A |
Normal Status |
|
Any switchable device that may participate in Phase Swap |
NormalPosition_B |
NORMALPOSITION_B |
Normal Status |
|
Any switchable device that may participate in Phase Swap |
NormalPosition_C |
NORMALPOSITION_C |
Normal Status |
Omit Features from Phase Swap
Assign the DISABLEPHASESWAP model name to any feature class that you wish to omit from Phase Swap. The Phase Swap tool will ignore any feature class with this model name assigned.