Add Domain

Extended Feeder Manager uses the standard Feeder Manager domains as well as the following Yes/No domain. Create the following domain.

Yes/No Domain

Properties:

  • Field type: Short Integer

  • Domain type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default value

Coded Values:

Code

Description

0

No

1

Yes

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?