Assign Model Names and Autoupdaters
Assign the following model names and autoupdaters. Model names are listed after the feature class.
The UFMVISIBLE model name determines which layers are visible when the user is viewing the manhole diagrams (i.e., precision drawing mode). Only layers with the UFMVISIBLE model name assigned will be displayed. You may wish to display other layers (e.g., conductor) while viewing underground diagrams. Assign this model name to these layers.
Cables (Primary, Secondary, Fiber): UFMVISIBLE
Conduit: UFMVISIBLE
Special Autoupdaters
Assign these autoupdaters on the Object Info tab of the ArcFM Properties Manager.
Feature Property |
Autoupdater |
---|---|
On Feature Update |
ArcFM UFM Conduit Cross Section |
Duct: UFMDUCT, UFMVISIBLE
Field Model Names
Field |
Field Model Name |
---|---|
PhaseDesignation |
PHASEDESIGNATION |
DuctPosition |
DUCTID |
DuctName |
DUCTNAME |
Available |
DUCTAVAILABILITY |
Occupied |
DUCTOCCUPIED |
DuctSize |
DUCTSIZE |
Material |
DUCTMATERIAL |
HasSubducts |
HASSUBDUCTS |
Special Autoupdaters
Assign these autoupdaters on the Object Info tab of the ArcFM Properties Manager.
Feature Property |
Autoupdater |
---|---|
On Feature Create |
ArcFM UFM Duct to Conduit Synch |
On Feature Update |
ArcFM UFM Duct to Conduit Synch, ArcFM UFM Resize Duct AU |
On Feature Delete |
ArcFM UFM Duct to Conduit Synch, ArcFM UFM Delete Duct Connector |
DuctAnnotation: UFMANNOTATION, UFMVISIBLE
DuctBank: UFMDUCTBANK, UFMVISIBLE
Field Model Names
Field |
Field Model Name |
---|---|
FacilityID |
FACILITYID |
DuctBankAnchor: UFMDUCTBANKANCHOR, UFMVISIBLE
Field Model Names
Field |
Field Model Name |
---|---|
SymbolRotation |
SYMBOLROTATION |
Split Information
Set this property on the Object Info tab of the ArcFM Properties Manager.
Feature Property |
Value |
---|---|
Split On Edit |
No |
The DuctBankAnchor feature class is only used when Conduit Manager creates a composite favorite. These features are never placed by the user. The Split On Edit property is set to No to prevent the potential for inadvertantly splitting a line feature.
DuctConnector: UFMDUCTCONNECTOR, UFMVISIBLE
Field Model Names
Field |
Field Model Name |
---|---|
PhaseDesignation |
PHASEDESIGNATION |
DuctDefinition: DUCT
Field Model Names
Field |
Field Model Name |
---|---|
DuctSize |
DUCTSIZE |
DuctNoteAnno: UFMANNOTATION, UFMVISIBLE
Splice: UFMSPLICE
UFMAnchor: UFMANCHOR, UFMVISIBLE
Field Model Names
Field |
Field Model Name |
---|---|
SymbolRotation |
SYMBOLROTATION |
Split Information
Set this property on the Object Info tab of the ArcFM Properties Manager.
Feature Property |
Value |
---|---|
Split On Edit |
No |
The UFMAnchor feature class is only used when Conduit Manager creates a composite favorite. These features are never placed by the user. The Split On Edit property is set to No to prevent the potential for inadvertantly splitting a line feature.
UFMFloor: UFMFLOOR, UFMVISIBLE
Field Model Names
Field |
Field Model Name |
---|---|
FacilityID |
FACILITYID |
UFMInsetFrameSource: INSETFRAMESOURCE, UFMINSETFRAMESOURCE
Field Model Names
Field |
Field Model Name |
---|---|
Title |
INSETFRAMETITLE |
UFMWall: UFMVISIBLE, UFMWALL
Field Model Names
Field |
Field Model Name |
---|---|
FacilityID |
FACILITYID |
UFMWall features must snap to the UFMFloor features. Use the ArcFM Snapping Manager to set this.

UFMWallDimensioning: UFMDIMENSION, UFMVISIBLE
UndergroundStructure: MANHOLEFEATURESNAP, STRUCTURE
Field Model Names
Field Name |
Data Type |
---|---|
FacilityID |
FACILITYID |
SymbolRotation |
SYMBOLROTATION |
FacilityDiagram |
FACILITYDIAGRAM |
Special Autoupdaters
Assign these autoupdaters on the Object Info tab of the ArcFM Properties Manager.
Feature Property |
Autoupdater |
---|---|
On Feature Update |
ArcFM Populate Facility ID |
Conduit_Cable relationship: (primary, secondary, fiber optic)
The autoupdater assigned below calls the ArcFM UFM Conduit to Conductor Relationship AU and the ArcFM Manage Conduit Manager Relationship Changes AU. It should replace the ArcFM Manage Conduit Manager Relationship Changes AU assigned during the basic Conduit Manager configuration.
Relationship Autoupdaters
Assign these autoupdaters on the Relationship Class Options tab of the ArcFM Properties Manager.
Feature Property |
Autoupdater |
---|---|
On Relationship Created |
ArcFM Conduit to Conductor Composite |
On Relationship Updated |
ArcFM Conduit to Conductor Composite |
On Relationship Deleted |
ArcFM Conduit to Conductor Composite |
ConduitSystem_DuctBank relationship:
Relationship Autoupdaters
Assign these autoupdaters on the Relationship Class Options tab of the ArcFM Properties Manager.
Feature Property |
Autoupdater |
---|---|
On Relationship Created |
ArcFM UFM Populate Conduit Blob on Duct Bank Relationship Creation AU |
Cable_Duct relationships: (primary, secondary, fiber)
Relationship Autoupdaters
Assign these autoupdaters on the Relationship Class Options tab of the ArcFM Properties Manager. These should be assigned to all Cable_Duct relationships (e.g., PriUGElectricLineSegment_Duct, SecUGElectricLineSegment_Duct, FiberCable_Duct).
Feature Property |
Autoupdater |
---|---|
On Relationship Created |
ArcFM UFM Duct to Conductor Relationship |
On Relationship Updated |
ArcFM UFM Duct to Conductor Relationship |
On Relationship Deleted |
ArcFM UFM Duct to Conductor Relationship |