Send Express Design to GIS

Identifies whether the user is in the field or on the enterprise and executes the appropriate task: Send Design to Enterprise or Send Design to Field.

Enabled

  • A design node must be selected.

Execute

  1. Checks to see if the user is in the field or on the enterprise.

  2. If the user is in the field, executes Send Design to Enterprise task.

  3. If the user is on the enterprise, executes the Send Design to Field task.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?