Send Session to Field

Takes a session from the enterprise server and puts it in the mobile environment.

Enabled

  • The Database ID field must have a value. This field is located in the Process Framework Administration Tool on the Extensions tab.

  • MMSessionManager must be the current extension.

  • The selected node must be a session.

  • The MM_Mobile_State table must exist in the current Process Framework database.

  • The current session must have not already been imported.

Execute

  1. Closes the session if it is open in ArcMap.

  2. Creates a mobile packet if one does not already exist.

  3. Saves the mobile packet.

  4. Adds the mobile packet to the transporter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?