Configure Heading Options

To configure the Heading Option for use in your geodatabase, follow these steps:

  1. Add the following model names to the Electric Object Class Model Name domain.

    ACTUALDUCTSIZE

    DUCTMATERIAL

    DUCTSIZE

  2. Add the following field to the DuctDefinition object class.

    Field Name

    Data Type

    Material

    text

  3. Assign the following field model names to the appropriate fields on the DuctDefinition object class.

    Field

    Field Model Name

    Field Editor

    ActualSize*

    ACTUALDUCTSIZE

     

    DuctSize

    DUCTSIZE

    ArcFM Duct Size Editor

    Material

    DUCTMATERIAL

     

    *The Heading Option functionality first looks at the ActualSize field for the size. If a field with the ACTUALDUCTSIZE field model name is not available, it retrieves the value from the DuctSize field.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?