Reconcile Design

Reconciles the parent version to the current design.

Enabled

  • MMWorkflowManager must be the current extension.

  • Workflow Manager must be open through ArcMap.

  • The selected node is a design node.

  • The user must have an editing session started in ArcMap.

  • A design must be open in ArcMap.

  • Reconcile target must either be default version or a postable version.

Execute

  1. Determines whether the DefineConflictsByColumn configuration value is set in the Process Framework Admin Tool. If this value is set to 1, conflicts are defined by column. If this value is set to 0 or not set at all, conflicts are defined by row.

  2. Reconciles the parent version to the open design.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?