Configure License Manager with Firewall

License Manager may be used with firewalls. If you use an enterprise firewall, License Manager communicates through TCP port 29001. If you have a personal firewall installed, you may need to configure the firewall application to allow network access to Miner.LicenseManagement.LicenseService.exe.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?